Already built the data logger using Stalker V2.
Using one lipo batt 18650 2200mAh and 3 solar cell (each 2volt 50mA max)
It run well about 2 days, but today i got the stalker stop working.
The led keep on, and the logger stop writing to the card.
When checking the log data, i got 25/45/165 on the date.
I don’t see where the problem is.
The temp seem correct, so the lipo voltage
6/11/11,13:29:2,46.69,4.16
6/11/11,13:29:4,46.75,4.16
6/11/11,13:29:7,46.75,4.16
25/8/165,13:29:9,46.75,4.16
6/11/11,13:29:11,46.75,4.16
6/11/11,13:29:13,46.75,4.16
6/11/11,13:29:15,46.81,4.16
6/11/11,13:29:17,46.81,4.16
25/45/165,9:29:19,46.81,4.16
6/11/8,13:29:21,46.81,4.16
6/11/85,13:29:23,46.81,4.16
6/11/11,13:29:25,46.81,4.16
25/45/165,45:85:85,46.88,4.16
6/11/11,13:29:30,46.88,4.16
25/8/165,13:29:32,46.88,4.16
25/8/165,13:29:34,46.88,4.16
25/45/165,45:85:25,46.88,4.16
6/11/11,13:29:38,46.88,4.16
25/45/165,45:85:45,46.94,4.16
25/45/165,10:29:42,46.94,4.16
25/45/165,45:85:25,46.94,4.16
6/11/11,16:0:11,41.25,4.11
6/11/11,16:0:13,41.19,4.11
The stalker, lipo batt, and the solar cell sit inside tight container using some of tupperware stuff (it’s fun using them, and cheaper)
Maybe the heat that generate this problem ?
I thought the stalker will survive about 80 degree C.
Maybe the voltage regulator keep the voltage up-high in the high temp ?
Maybe i will toast them in the oven (like i did with duemilanove, and it fail) to test the high temp.
need more infos…
thanks for reading