The Stalker V2.1 I just received is not working. I’m using Linux Ubuntu 11.04. and Arduino IDE 0022. The Stalker shows up in the Arduino IDE: Tools -> Serial Port -> /dev/ttyUSB0
I downloaded the DS3231 library and Datalogger Sketches from the resources section of the Stalker V2.1 WIKI http://www.seeedstudio.com/wiki/File:SeeeduinoStalkerV2.1_Software.zip
I moved the unzipped file to the location with all the other examples: /usr/share/arduino/libraries
So I now have a folder called DS3231, then did the following.
-
Inserted the RC2032 Battery, positive side up into the Stalker.
-
Set UartSBee onboard voltage regulator switch to 5 volts.
-
Connected a 6 pin ribbon cable “No crossed wires” from the Stalker to the UartSBee.
-
Connected the USB cable from the UartSBee directly to my PC. “No USB hub”
-
In Arduino IDE: Tools–>Board -> Arduino Pro or Pro Mini (3.3V, 8MHz) w/ ATmega 328
6 In Arduino IDE: Tools -> Serial monitor “57,600 baud, no autoscroll, no line ending” “I also tried 4800 baud”
-
In Arduino IDE: FILE -> Examples -> DS3231 -> adjust.pde
-
In Arduino IDE: Verify
-
In Arduino IDE: Upload
I get the following error:
avrdude: stk500_getsync(): not in sync: resp=0x00
Would you please post the connect picture?
I see now the problem is the connections. I assumed that the connections would match up but they don’t and I didn’t check them. I can’t understand why it would be made this way. I ordered the parts the WIKI page said to order: Stalker V2.1, UartSBee and a ribbon cable. But the ribbon cable didn’t fit. 8 emails later I was finally able to communicate the problem and get a cable that will work shipped to me but still haven’t received it yet. The cable I’m using now I made myself. I see now the WIKI has been changed to show 1-pine dual female jumper wires instead which aren’t very convenient to use for this. Not a great way to start off with a new customer. I had this thing for a month now and haven’t been able to use it.
So is this correct?
Stalker : UartSBee
DTR -> DTR
TXD -> TX
RXD -> RX
USB5V -> VCC
GND -> GND
GND -> CTS ???
connect as:
Stalker : UartSBee
DTR -> DTR
TXD -> RX
RXD -> TX
USB5V -> VCC
GND -> GND
GND -> CTS
And toggle the UartSBee switch to 5V side.
Yes I did set the switch to 5V as I listed in step 2 and by process of elimination I figured it should be GND -> CTS but just wanted to make sure. Thank you.
Perhaps future generations of either the Stalker or UartSBee can be made so the pins match up.