Hi there, as a nub’ in *bee I’ve try to use the given pde in the wiki, but that give me an error when compile. I past the code just for you ain’t search:
#include <NewSoftSerial.h> //Software Serial Port
#define RxD 11
#define TxD 12
NewSoftSerial blueToothSerial(RxD,TxD);
void setup()
{
Serial.begin(9600); //Serial port for debugging, Comment this line if not required
pinMode(RxD, INPUT);
pinMode(TxD, OUTPUT);
setupBlueToothConnection();
}
void loop()
{
if(blueToothSerial.read() == 'a')
{
blueToothSerial.println("You are connected to Bluetooth Bee");
//You can write you BT communication logic here
}
}
void setupBlueToothConnection()
{
Serial.print("Setting up Bluetooth link"); //For debugging, Comment this line if not required
blueToothSerial.begin(38400); //Set BluetoothBee BaudRate to default baud rate 38400
delay(1000);
sendBlueToothCommand("\r\n+STWMOD=0\r\n");
sendBlueToothCommand("\r\n+STNA=modem\r\n");
sendBlueToothCommand("\r\n+STAUTO=0\r\n");
sendBlueToothCommand("\r\n+STOAUT=1\r\n");
sendBlueToothCommand("\r\n+STPIN=0000\r\n");
delay(2000); // This delay is required.
blueToothSerial.print("\r\n+INQ=1\r\n");
delay(2000); // This delay is required.
Serial.print("Setup complete");
}
void sendBlueToothCommand(char command[])
{
char a;
blueToothSerial.print(command);
Serial.print(command); //For debugging, Comment this line if not required
delay(3000);
while(blueToothSerial.available()) //For debugging, Comment this line if not required
{ //For debugging, Comment this line if not required
Serial.print(char(blueToothSerial.read())); //For debugging, Comment this line if not required
} //For debugging, Comment this line if not required
}
then this is the error it give me
I understand that 1st problem is that the *.h missing file, must’n I load it two file, like for compiling a regular software.
If some one have alike for a basic tutorial to use a bluetooth-bee with the bee connector on this board, I’m interested too, ![]()
Thanks to have read me