Stable WiFi ntp failing

Hi. Yes that seems to be the issue.

I have TWO SSID’s. The actual names are ‘George’, this is the 2.4Ghz and ‘Mildred’ is the 5.0Ghz. These are specific names I gave them when I configure my router.

They both use WPA2-PSK. Mildred is fixed to Channel 44 and George is set the Auto so will vary.

I have been using George up until now as the signal strength is better where I have the WIO Terminal positioned.

However now it does not list George. The Laptop sitting next the the WIO Terminal lists and connects to Both George and Mildred.