I just bow one DSO Quad and I am a newbbie.
sorry, but is it possible to encrease the reading speed?
I wold like use the DSO Q. to see a signal at 19.1 - 19.9kHz, I do not need to have a really accurate measure, I want just see that and I need to know when the signal pass … that’s the problem, the signal is not costant (it is a data communciation) and so my DSO have not enought time to show that correctly. I have to know exactly how many data packs are passing so I cannot see any single wave modifing the speed to some microseconds, but I have to read the line at 100ms (each data pack spend about 10-100ms to pass) and due the DSO delay I cannot see anything with sense.
please, do you know any “tricky”?
really really thank’s in advance.
Drugo