Hello,
Both Windows and Linux show Speakers as an output device, of course there are no speakers, so what is the OS detecting?
Thanks!
Hello,
Both Windows and Linux show Speakers as an output device, of course there are no speakers, so what is the OS detecting?
Thanks!
Sorrry, I didn’t get your point.
@Bruce.Qin The os detects speakers in the Odyssey, they are displayed in the sound devices - realtek speakers - what are they?
Thanks
It‘s just diaplay the codec name.
so there are no speakers, I thought it could be something like an internal beeper?
Thanks @Bruce.Qin
Ahh,without internal speaker. 
Ok - so it must be something to do with Linux, I wonder if others have the same.
Thanks!
You can add a buzzer and use a gpio to control it in linux.
Thank you @Bruce.Qin
I am mainly trying to understand why Linux shows two analogue outputs instead of a single one.
How about in your Linux setup, do you have one to check?