Speaker not working

Hi Alden,

you can probe the pins directly on the Xadow Audio and the Xadow GSM breakout

As shown in the image below, if you let the Xadow GSM breakout jump in where between the touchscreen and the Xadow GSM+BLE, then the “Probe test 1&2” checked the connection between the Xadow GSM breakout to touchscreen and to the Xadow Audio.

The SPK_OUT_N and SPK_OUT_P refer to D2 and C2 respectively on the Xadow GSM breakout, check below:

if the speaker is working well, “Probe Test 3” should tell you an impedance of speaker at about 8 ± 20% ohms.