I just got the board Spartan 7 accelerator plus seeduino v4.2 .
I have managed to run the bitstream that I created on Vivado like Rgb leds etc .
The problem is that the seeduino v4.2 doesn’t blink the leds or rgbs for that mater in other hand as soon as I install the Spartan 7 on a arduino uno board it’s works fine both uno and seeduino have the same code installed so definitely this seeduino is a bad board and choice in my opinion .
I was wondering if anyone else had this issue . And if any one else had returned the board to the makers which is not so good to begin with as just few days of operation it went bust