Hello,
I’m trying to play a bit with my UartSB v2.2, but I’m having some troubles.
To start, I just wanted to use an Arduino to emit some data on the serial port, and using UartSB to receive them on my computer - and use a simple program like cutecom to read the data.
I set up the Arduino to produce a stream of data, then I connected arduino Tx to UartSB Rx and vice-versa. But I can’t read anything.
I’m on a Linux box (Fedora 13, to be precise) but I think there are troubles in detecting the device, because dmesg says:
No matter which port I am using, I get this message. On a forum I found that it may be necessary to load the module ftdi_sio to FTDI chips to work properly. I did it, but dmesg still giving the same result.
In addition, none of the /dev/ttySx port is working, nor any is created/removed when plugging in/out the UartSB (but this seems obvious as the device isn’t detected).
None of lsusb or usb-devices list the UartSB.
I’ll try on another computer later, but for now… Any help is appreciated!
Thanks in advance ![]()
~Aki