Hello,
I use Grove Serial Bluetooth module + Arduino Mega 1280.
I try to communicate my Android phone (Samsung GS2) with my arduino.
On my Android phone I use the following application “S2 Bluetooth Terminal3” or “BlueTerm”
On the Arduino, I loaded the Bluetooth demo code (slave).
The bluetooth connection is done and I got the message “The slave bluetooth is inquirable!” on my phone when the Arduino start. So the communication Arduino->Phone is correct.
The problem is that I don’t receive anything on the Arduino board when I send data from the phone !
(I tried to sent data from my phone to a BT computer, with the same applications, and it works).
Any idea ?
The demo code I use :
#include <SoftwareSerial.h> //Software Serial Port
#define RxD 6
#define TxD 7
SoftwareSerial blueToothSerial(RxD,TxD);
void setup()
{
Serial.begin(9600);
pinMode(RxD, INPUT);
pinMode(TxD, OUTPUT);
setupBlueToothConnection();
}
void loop()
{
char recvChar;
while(1){
if(blueToothSerial.available()){//check if there's any data sent from the remote bluetooth shield
recvChar = blueToothSerial.read();
Serial.print(recvChar);
}
if(Serial.available()){//check if there's any data sent from the local serial terminal, you can add the other applications here
recvChar = Serial.read();
blueToothSerial.print(recvChar);
}
}
}
void setupBlueToothConnection()
{
blueToothSerial.begin(38400); //Set BluetoothBee BaudRate to default baud rate 38400
blueToothSerial.print("\r\n+STWMOD=0\r\n"); //set the bluetooth work in slave mode
blueToothSerial.print("\r\n+STNA=SeeedBTSlave\r\n"); //set the bluetooth name as "SeeedBTSlave"
blueToothSerial.print("\r\n+STPIN=0000\r\n");//Set SLAVE pincode"0000"
blueToothSerial.print("\r\n+STOAUT=1\r\n"); // Permit Paired device to connect me
blueToothSerial.print("\r\n+STAUTO=0\r\n"); // Auto-connection should be forbidden here
delay(2000); // This delay is required.
blueToothSerial.print("\r\n+INQ=1\r\n"); //make the slave bluetooth inquirable
Serial.println("The slave bluetooth is inquirable!");
delay(2000); // This delay is required.
blueToothSerial.flush();
}