Hi,
I bought a CUI32Stern and I’m a newbee in µC programmation (but experienced inPHP/javascript). I would like to know what’s the easyest way to program my CUI32 ? I would like to use an accelerometer, gps.
I have installed MPide but when I verify a code (examples code) it always return :
C:\Program Files (x86)\MPide\hardware\pic32\cores\pic32\HardwareSerial.cpp:670:60: error: Interrupt priority must be specified as ‘single’ or ‘IPLn[AUTO|SOFT|SRS]’, where n is in the range of 0…7, inclusive.
C:\Program Files (x86)\MPide\hardware\pic32\cores\pic32\HardwareSerial.cpp:698:60: error: Interrupt priority must be specified as ‘single’ or ‘IPLn[AUTO|SOFT|SRS]’, where n is in the range of 0…7, inclusive.
Thanks for help