The SkyConnect page claims it is “…compatible with Zigbee/Thread/Matter,…” But Zigbee is not just a protocol, it’s a hardware spec, too, where Thread and Matter are hardware agnostic. This is kind of explained by the mention of the multi-protocol radio MCU, but only if the reader knows what that means.
Along with throwing out industry buzzwords like a wood chipper, the description is full of flowery, meaningless phrases. “The drive supports full-speed USB 2.0 when plugged into the included USB extender.” Um… wow? And probably grandstanding a bit, since this next one plainly states it’ll be limited by the serial chip: “Direct local serial communication will be done via an onboard USB-to-UART bridge/converter (presumably a chip in Silicon Labs CP210x series).” Not only does this give zero information to readers, the Silicon Labs CP210x chips are extremely hard to get right now, so that presumption is, presumably, false. And do you know any USB to UART bridge chips that can handle full speed USB 2.x for any longer than it takes to fill their tiny buffer? Hence, meaningless.
Seeed Studio customers are Makers. Above all, Makers seek knowledge, and are typically put off by buzzword spewing, flowery descriptions that have no bearing on our craft. How about a little more information-leaning text and a little less sales pitch?