SiPeed MaixCube built in applications

I have just received my RiscV MaixCube, and I like the built in applications, but at the moment they seem to be a bit immature… The camera image is reversed left to right on the built in screen. Also, the only way out after having taken a single shot, is to reset the device. The image doesn’t seem to be stored anywhere, and if I put a microSD card in, the device seems to crash on start-up. Has anyone got any further with the as delivered firmware?
Tony


This is our supplier from the product, they want to focus the discussion on their forum.

Thanks - I’ll repost there.
Tony