SIM900 Mini Firmware Update Error

Have 2 SIM900 Mini V3.8.2 Modules. Successfully updated the firmware on one, following the steps here:

http://acoptex.com/wp/basics-project-105b-sim900a-gsm-gprs-module-how-to-flash-another-firmware/

But the other module cleared the flash but when it went to write the new firmware it shows the “ERROR Set writing flash error! (264)”. I couldn’t find any help manuals or posts about error 264 except this one: http://amichalec.net/2014/08/03/sim900a-fixed-for-europe/
where a guy in the comments asks about this error with no response. Any help or link to the developer of the “SIM900 Series download Tools Develop 1.9” software would be greatly appreciated

UPDATE
I tried to use the other software recommended by the guide i followed above “Simcom - sim900 Customer flash loader V1.01” and it just worked. Same setup just different software worked for one board. Hope this helps someone

https://wiki.seeedstudio.com/GPRS_Shield_V3.0/#hardware-overview
I don’t see anything in the wiki that says you need to update the firmware to use it.

1 Like

Indeed you do not for a lot of the features. I was able to use the factory firmware just fine. However i was wanting to sending data to a “https” server not just “http” and for this a firmware update was required.

I had the same issue. Then I tried “SIM900 Customer flash loader V1.01” but also got errors. Then I changed the speed in “SIM900 Customer flash loader V1.01” to 115200 and it flashed successfully.

There is a known issue that in some cases the Genie Mini firmware update will fail and you will be prompted with a ‘Failed Firmware Update’ error message. In this situation, the Genie Mini charging indicator LED will flash red, indicating that the device is in SAFE mode as there is no firmware currently loaded. The battery indicator will have a question mark and read as empty - this doesn’t mean there is an issue with the battery, it’s just a response to the firmware error. Please follow the steps below to get back up and running.

Please click here to troubleshoot firmware update failures on Genie Mini II, Genie II Linear or a Genie II Pan Tilt.

Before you start, make sure you:

turn Wifi off on your device
disconnect from a VPN (if you are using one)
disable any anti virus software on your device,
make sure your device is not connected to other Bluetooth devices during the update process,
turn Bluetooth off on other devices in range, including Bluetooth speakers, headphones, smart watches, fitness trackers and other Genie Minis,
try the update in a different location - we have heard of situations where there can be interference in certain locations,
try the update on a different device - you will be able to go back to your original device if the update is successful.
Forced firmware update - iOS:

plug the Genie Mini in to power,
force close the App and reopen on your device (double tap the home button and swipe upwards),
now navigate to the Connection Screen on the App at the top right.
hold down the Genie Mini’s ON button for 10 – 15 seconds (this resets the hardware - a series of lights will flash),
you will see the Genie Mini appear in the Connection Screen. Tap to CONNECT,
the battery symbol at the top right of the screen will show a question mark as the battery levels can’t be read in safe mode,
navigate to the New Time Lapse screen and select New Time Lapse,
this will prompt a firmware update. Update your device,
Forced firmware update - Android:

plug the Genie Mini in to power,
force close the App and reopen on your device (tap the overview button to close the App),
now navigate to the Connection Screen on the App at the top right,
hold down the Genie Mini’s ON button for 10 – 15 seconds (this resets the hardware - a series of lights will flash),
you will see the Genie Mini appear in the Connection Screen. Tap to CONNECT,
navigate to the SETTINGS menu and tap FIRMWARE RELOAD,
this will prompt a firmware update. Update your device,
once the firmware has updated, restart the App.

This may help you,
Rachel Gomez