Hi,
I’m putting together some circuit boards that I’d like to chain together in the same manner as the Rainbowduino.
In order to do this I need some single-row right-angle female headers. So far as I can tell Seeedstudio don’t sell these in the depot, although they stock right-angle male headers.
Given that a picture means a thousand words – here’s what I have in mind:

The Rainbowduino (as pictured) uses an 8 pin version of these. My project currently calls for one 4 pin and one 6 pin header per board.
Is there any chance that Seeedstudio could add a range of these headers to the depot? As I say, I need 4 pin and 6 pin versions, but I’d imagine a range of say 2, 4, 6, 8 and 10 pin versions could come in really handy. At a pinch, I could rework my design to use the 8 pin versions that the Rainbowduino uses, if they’re more readily available.
Cheers,
blue.zener