Significant issues with the SenseCAP Watcher

I purchased the Watcher through the official Seeed Studio website, and it currently cannot perform the desired functions.

  1. Device Registration:

After downloading the SenseCraft Mate app on my iPhone 15 Max and attempting to register the device via QR code, I receive a message saying the device has been added. However, the registered device does not appear on the device registration screen (attached photo).


  1. Connection to MacBook:

After connecting the Watcher to my MacBook with the included USB cable, I tried connecting to the serial port on the SenseCraft website, but it couldn’t detect the serial port (although it is visible in the Arduino IDE).

It seems it may not be the right time to purchase… The pre-installed AI models work fine.

3 Likes

SenseCraft Mate app should have the necessary permissions on your iPhone (e.g., Bluetooth, location, etc.). Please recheck these options.

2 Likes

Unfortunately, all permissions have been applied.

Hello, I am the application engineer responsible for the SenseCAP Watcher product. We take your feedback very seriously and apologize for any inconvenience caused. Please send me a private message to the body EUI behind Watcher, we will check the situation of your device in the background and help you solve the problem as soon as possible, please pay attention to the private message I sent you.

3 Likes

I sensed message thanks!!

connected!! thank you! thank you! bro!!

1 Like

We are glad to help you, thank you for your support of our products, and wish you a happy life.

1 Like

I’m having a similar issue. The app says that the device is connected however it’s not visible I’m devices and setting it up manually stays on page 1 and is unable to continue to configuration.

Hello Citric! This is C2G, I have exactly the same problem as [byeongyeong_choi] with the same notification message in the IOS app as in the screenshot. Nothing else happens. I also checked the permission of the app. Can you help me? This would be great…

Same problem. How can I solve that?

Hello everyone, when binding the SenseCAP Watcher, please ensure that you have selected the correct region: Global. Then proceed with registration and login, otherwise it may result in binding failure. If you still cannot bind the device, please send your device information to [email protected], and our technical support team will assist you in resolving the issue. Thank you for your understanding and cooperation.

1 Like

Hi, I’m currently facing similar issue as well. Using POCO F5 Pro phone. The OS is Xiaomi HyperOS 2.0.5.0.

The SenseCraft account is registered under Global server as well.

Citric, I need help with my device. It just can’t do the firmware update. Therefore, nothing is working. The device I new (1 day after received)). Can you help me?

Significant issues with the SenseCAP Watcher - #12 by Citric?

the email is the best because you can get directly to Sensecap engineers. I am sure Citric would be happy to help but he is a VIP this way, you understand I am sure…

also for reference you probably should not try a firmware update right out of the box… you should play with it first before

firmware upgrades are a privlage not a right… please keep this in mind, because otherwise they will not support firmware updates because customers brick their own devices and blame the manufacturer… so it is important to be a good community member

Hello! I also have the problem that I can’t connect to the phone app! The process starts, it connects to wifi, but for some reason it never succeeds until bind. Xiaomi 15 U, Android 16. Can you help me solve this problem?

Same here i ha e 2.4 GHz but not binding with Samsung Gal s22

Hi,

I am experiencing the same issue. I have received the product today through an e-commerce website in the Phl and was shipped from China.

After scanning the QR code there’s an issue with the EUI Key error. While there’s no issue manually entering the EUI & Key, the device remains offline and has no connection through wifi or is not automatically connecting to my mobile device.

1 Like

I’m having an activation issue. I activated my device via my phone and wanted to download the agent because it didn’t come with one. I created the agent on the website, but when I tried to download it, I was asked to enter a six-digit code. Watcher didn’t show it, so I thought I needed to update the firmware. So, I clicked “Update.” I installed the Xiaozhi firmware and received an activation code, but when I tried to enter it, I got a message saying the device was already activated. That’s it, I can’t use it at all. It turns out I replaced the default Watcher AI firmware with Xiaozhi, and now nothing works.

2 Likes

try 123456 as the code

I have a code written down on my Watcher. It’s not accepted on the sensecraftai website. They say the code is invalid or the device is already activated.

2 Likes