Hi I have a pretty old shield bot (2012) and my right motor doesn’t work; I can power it from a 5V source and if I turn it it will give power to the arduino, I tested continuity and it’s fully connected to the servo driver chip. I tried with a seeduino but it will still not work
Have any idea ?
PS: I’m new to arduino and coding so please don’t use too complex language, thank 
Hi there~,
- you can use the 1.5 battery and connect it to motor 2 pads directly to check if the motor moves. If it does not move, the motor maybe bad. If it moves, it will be related with seeeduino code.
- You can follow
<LINK_TEXT text=“http://wiki.seeedstudio.com/Shield_Bot_ … ng-started”>http://wiki.seeedstudio.com/Shield_Bot_V1.2/#getting-started</LINK_TEXT> to burn the code.
- I record a video about the example. thanks.
<LINK_TEXT text=“https://github.com/SeeedDocument/forum_ … eldBot.mp4”>https://github.com/SeeedDocument/forum_doc/raw/master/image/ShieldBot.mp4</LINK_TEXT>
Thanks for responding, I tried to power the motor with 5V and it works, I also tried to write my own code but it still doesn’t work.
Hi there~
- If you burn the below code to shield bot, both of the motors shall rotate.
<LINK_TEXT text=“http://wiki.seeedstudio.com/Shield_Bot_ … ng-started”>http://wiki.seeedstudio.com/Shield_Bot_V1.2/#getting-started</LINK_TEXT>
- If it does not rotate, the shield bot may be bad from hardware point of view. The motor is connected with L298 and then controlled by arduino through IN1/IN2/IN3/IN4 and ENA/ENB. We suspect the L298 is dead. thanks.