Hi liaifat85,
AT+MODELS?\r showed only one position (id:1):
{“type”: 0, “name”: “MODELS?”, “code”: 0, “data”: [{“id”: 1, “type”: 0, “address”: 4194304, “size”: 0}]}
I’ve uploaded ‘Gesture Detection’ (Paper, Rock, Scissors) using SenseCraft AI web interface.
Do you mean that Grove Vision AI Module V2 with default FW has only one slot for the models ?
If yes - is it possible to update FW (or maybe some manipulations using AT commands) to get at least 2 slots ?