Setting volume on 5w speaker output on ReSpeaker Lite

So I’ve had great success with ReSpeaker Lite in my Home Assistant environment. The adoption to ESPHome is simple, the built-in wake words seem to have a better pickup distance than the 3m advertised, and by including some LLM I’m close to severing the Amazon Alexa connection. I’ve used CAD to build 3d prints for both a standalone case and a case with a 2" speaker housing that I can flush mount to my walls and use PoE to USB for power. I have 2 challenges I’m seeking to resolve:

  1. At max output the speaker is a bit loud and has enough distortion that I’d rather just bring it down around 30-50%. I’m sure I can figure something out schematically to reduce the volume, but I was hoping there was a i2c switch or something that I could put in the config to take it down a notch.
  2. I’d love to be able to use the ReSpeaker Lite as a media satellite but I don’t see much out there as far as the process by which I can make this happen. If it can’t, no worries. I’m good with resolving 1 and letting music playback happen through other means.

Hi there,
This is cool stuff can you provide more info? “How to” ON the ESP Home front. What guide did you follow or steps to take could you recommend to a New ESP home install?
I believe many would benefit from such info.
TIA

GL :slight_smile: PJ :v:

would be extra points if you can share the 3D prints here too! I post a ton of freeCad and Gcode prints for stuff like the Xiao dIY- Socket very well received. so much so I keep getting gifts in the post! LOL :smile: