Hi Experts,
I am looking for a SERVO Controller that can be driven from a GROVE-XIAO shield and that can drive 4-6 Separate Servos. Servo controller should be connected to the same LIPO battery(3.7V), but SERVO Controller may need to output between 3.3-7.4 Volt depending on the SERVO attached to it, like the picture below… I do not want to redesign a Servo Controller. I have space limitations…
Please provide some suggestion that will require minimum work to hook up with a XIAO shield…