Hi @ernieboxer
Our ODYSSEY board wants the fan to rotate with a minimum temperature threshold of 40°C. When the CPU temperature is lower than 40°C, the fan will stop rotating. Although you cannot keep the fan running all the time, you can speed up the fan speed by 20%. You can set it through chipset—>FAN Control—>Positive.