I was trying to run the Wifi example provided in secton 5.3 of the official Developer’s Guide.
However, I can see nothing from the Serial Monitor in the Arduino application, nor any errors show up.
The Arduino version I use is 1.5.8, I tried this on a 64-bit Windows 7 as well as a 32-bit Windows XP, both resulted in the same behaviour. So my question is: is there any particular setup I need to make serial working here?
I have the Linkit USB ports appearing correctly when Linkit one plugged in to my PC viewed by Device Manager.
Can upload programs but it locks the Linkit and ports disappear on end of upload reset?
Reset at any time also generates a port loss and locks linkit.
Linkit can be recovered by resetting on battery or plugging into my laptops USB.
Uploaded program then functions.
reconnection back to PC USB, ports appear OK.
In Summary ‘Reset’ of LINKIT one connected to PC USB loses ports and locks Linkit?