I can’t get this form of the slcd.print function to work - slcd.print(float_data,2);//show float data,Decimal digits(1-3)
When I try slcd.print(float_data,1); it  hangs an Arduino 1.0.
I can’t confirm this. I use this code:
#include <SoftwareSerial.h>
#include "SerialLCD.h"
SerialLCD slcd(11,12);
void setup() {
  slcd.begin();
}
void loop() {
  slcd.setCursor(0, 1);
  float x = 754.321;
  slcd.print(x, 2);
  slcd.print(x, 1);
}
What version of SerialLCD library did you use? The one for arduino 1.0?
seeedstudio.com/wiki/images/ … ialLCD.zip
Any error message from arduino ide?
I tried using the library that you referenced and it does fix this problem. However, a new one now occurs with another form of slcd.print. This time, slcd.print(digits, DEC);, where “digits” is declared integer, will not compile. The error is:
call of overloaded ‘print(int&, int)’ is ambiguous.
This function worked with my other library but doesn’t now. I’m using Arduino v 1.0.1. Any ideas?
Yeah, i also get this error.
Take a look in SerialLCD.h:
void print(uint8_t b);
void print(const char[]);
void print(unsigned long n, uint8_t base);
void print(float data,uint8_t num);
no procedure for integer, but just convert it to unsigned long.
Hi,
Anyone know how to resolt   scld print float in Serial LCD V1.1? I try whit diferents librarys but dosen’t work.
I can show float in the serial port but the same instruccion, change serial.print for slcd.print it’s not working.
slcd.print(float_data,2);//show float data,Decimal digits(1-3)
Thanks for your time.