john
1
Does anyone know what the pinout on the serial interface of the Stalker is?
It’s not in the PDF and the diagram isn’t readable. Maybe there’s a document I missed?
(Also – I’m assuming that the stalker takes 5v on serial, not 3.3 like the xbee and bt modules?)
min0n
2
hi,
from up to down:
dtr
gnd
rx
tx
5V
you can see on this photo:
flickr.com/photos/min0n/4419133607/
john
3
excellent! is it listed anywhere? i wonder how I missed it. two more questions:
- can you do it without dtr (just powercycle the stalker after upload?)
- if i hook up correctly, can i just upload to the stalker without any other major steps?
the pins is
dtr
gnd
rx
tx
5V
and it’s correspond with UartSB