I have a problem with my Sensor Hub - 4G Data Logger.
I try to connect with sim roaming netmore and with other data sim, but after 94s resulti is your sim is expired, why???
Have a solution?
In this Sensor Hub - 4G Data Logger is possible to debug modem quectel with at command from debut uart connector?
Hey there,
Thank you very much for choosing SenseCAP. This is Violet from Seeed. Apologies for the inconvenience. This might be because the roaming function is not activated yet. We will upgrade the firmware via OTA in the near future. At the current stage, could you please download the new firmware from this Github link. And please let us know if the problem remains.
This is Jenkin, pls try to update the firmware again. Download from the link https://github.com/Wvirgil123/sensorhub , the version still 2.0.4, but we add some logs about sim card connection.
Hi Gabriele, for SenseCAP Sensor Hub, the default data upload interval is every 60 minutes. And if you would like to configure it to different intervals, please kindly refer to this user guide. It should be in Chapter 4.4.1.
Let us know if you need any further support. Thank you!