How or where do I get the SenseCap Watcher or do I have to wait till its launched on Kickstarter?
Good Question… I am not sure
Hi there,
I won one on the live stream, and I pretty sure ERic said 2 weeks before final unit design will start shipping.
I definitely want another, wonder how much?
HTH
GL
PJ
![]()
Get aboard the next live stream you can win one or some heavy discounts too. ![]()
Thanks all, hope to get it soon
Hi there,
yes jump in the beta trial if you have an Idea for a use case they maybe can get you one sooner.
This thing is GREAT! I really like it all in one like this.
HTH
GL
PJ ![]()
I’m waiting for my Watcher to arrive today. As soon as I get it, I’ll post my findings on Hackster.
@PJ_Glasso did you already connect serial terminal to the watcher? There is a console command terminal which has a lot of functions.
Hi there,
Yes I got something , but probably the wrong buad rate.
basically it’s on Charging It does the picture taking but I’m trying to have it Identify a properly cooked pizza, so I need to train the model and make some pizza’s LOL
just messing. It’s a nice device we’ll see time permitting how user friendly it can be for uploading pictures for some models etc. The menu system is a little meh’ they need to use the wheel and the touch screen for the circle gesture.
Still playing but definitely a good package
GL
PJ ![]()
I was plugged into the bottom usbC btw? terminal 9600 com30 LOL ![]()
Watch this:
Hello @PJ_Glasso,
Are you are still stuck with the watcher console?
If so maybe my recent post on Hackster can shed some light:
Hello, I just received my Watcher and I was unable to connect the camera to Home Assistant. All I could do was receive an Alarm Triggers when a pet was detected. Has anyone managed to do this?
Is it required to install SenseCraft on my own server? What if I want to use something else other than OpenAI or if I want to change the AI prompt?
Hi all! I’m building a hobby voice-assistant project.
The device should talk only to my home server over LAN — no direct internet dependency from the device side, all the AI orchestration happens on my server.
I’m using xiaozhi-protocol with my own gateway, and now I want to add vision capability. SenseCAP Watcher looks ideal — camera + Himax SSCMA integration, and the sensecap-watcher board is already in upstream 78/xiaozhi-esp32.
Before ordering, a few questions to de-risk:
Hardware revision: are units shipping today still v1.0, matching what’s in the OSHW repo and the upstream board files? Or has there been a v1.1+ I should be aware of?
Boot security: is secure-boot V2 or flash encryption enabled at factory? I want to confirm I can flash custom firmware via standard esptool.py and recover from factory_firmware.bin if needed.
Alternative path: if upstream xiaozhi-esp32 turns out not viable for some reason — is there a way to keep stock SenseCAP firmware but point its AI/voice traffic at a self-hosted endpoint instead of sensecraft.seeed.cc? I see HTTP-Proxy notifications in the docs but that seems to be for alerts only.
Either path works for me, just checking before placing the order. Thanks in advance! ![]()
Hardware revisions are usually minor PCB or component changes. Confirm current PCB revision and camera sensor compatibility. Secure boot and flash encryption usually disabled by default.