Hi there,
I tried to apply the firmware update from version 1.4 (I think) to 2.2 (I think) today. The process started by erasing the existing firmware. After that, it started flashing the new firmware. However, the flashing failed at around 21%.
Now the tracker seems to be broken. The LED blinks constantly every 2 seconds (1 second on, 1 second off). The device is visible as a Bluetooth device named “SENSECAP_GR_DFU_801975”. I tried several button press durations and combinations, but this behavior can’t be changed. Not even exited, i.e., I can’t turn off the sensor.
The app is able to connect to this device for another firmware upgrade. However, I am faced with only one option, namely “upload Firmware File”, where it wants me to select a local file to upload. I don’t have any such files, and I can’t find a place to download it online.
Can the support team please provide a firmware file?
Got my T1000-A today and first thing in the “sensecap mate app” was a hint of firmware upgrade (1.4 to 2.5). Started the upgrade, flashing after erasing finished 100%. After that a “failed” appeared.
Since then the same status as @TomStein. How to resolve this?
Hi there,
So I asked the Great “G” ----> sensecap version 1.4 download
It replied with 2 links , The first is a source for the files to download…
the Second was Your link here asking the Q. LOL
Idunno if it helps but here is what I found.
I tried searching all over the web, SeeedStudio support is not responding as well, and so I decided to reverse engineer, I was able to extract the firmware and restore my device. My tracker is now working perfectly
Thank you @cgmisola , after several attempts provided firmware will load, and t1000 will reboot with 2.5 firmware! Be aware to update with your phone close to the t1000, without any other bluetooth interference!
I tried to find the T1000 A/B v2.8 firmware to manually update my devices. The manual update was suggested from sensecap support to get back to be able to configure the devices after the update via app/download.
Where can I find the T1000A/B 2.8 firmware to download?
If your T1000 device gets stuck during the firmware update process and enters DFU mode, please contact our technical support team at [email protected] for the latest firmware to flash it manually!