SenseCAP T1000-E Meshtastic Tracker User Guide

SenseCAP T1000-E Meshtastic Tracker User Guide - Part1 Unboxing Setup

This is a video showing the unboxing and setup process for the T1000-E, to help you get started with Meshtastic quickly.

SenseCAP T1000-E Meshtastic Tracker User Guide - Part 2: Status Indicators of the T1000-E

In this video, we pick up where the last one left off, providing a step-by-step demonstration of the various status indicators of the T1000-E. You’ll learn how to power on, send and receive messages, charge, restart the device, enter DFU mode, update node/location information, toggle GPS on and off, and power off. If you’re new to Meshtastic or the T1000-E, this video is a great place to start. Check out the important timestamps below: 0:11–Power On 0:25–Working 0:34–Receive Message 1:29–Send Message 1:58–Charging 2:17–Restart 2:44–Enter DFU Mode 3:14–Double press the Button 3:28–Triple press the Button 3:40–Power Off

SenseCAP T1000-E Meshtastic Tracker User Guide - Part 3: Flash New Firmware

SenseCAP T1000-E is a high-performance tracker designed for ‪@Meshtastic‬ as small as a credit card, effortlessly fitting in your pocket or attaching to your assets. It embeds Semtech’s LR1110 (Supports 863-928 MHz range), ‪@NordicSemi‬’s nRF52840, and ‪@mediatek‬’s AG3335 GPS module, providing Meshtastic users with a high-precision, low-power positioning and communication solution. In this video, you’ll be walked through to flash a new Meshtastic firmware for this tracker.

1 Like