When using the iOS SenseCAP Mate app, the S2120 weather station will give the average wind speed and the highest wind gust since the last transmission. However, when it sends the LoRaWAN packet, it only gives the current wind speed at the moment it transmits. Having the average and the highest (gust) wind speed between reporting is essential. Is there a planned firmware update that might add this?