SenseCAP S1000 V2 10-in-1 Compact Weather Sensor wind speed incorrect

Hello,

I have a SenseCAP S1000 V2 10-in-1, wind speed does not seem to go above 2.5 m/s whereas it should reach at least 25/30.

Would you have an idea?

thanks

The wind sensor should be placed in an open area where it can measure the wind speed unobstructed.

it is the case. An anemometer measures properly.

I wish we could get better support for these devices… What Da? I think that device uses the dopplar method instead of the old fashon

Hello, could you please contact our technical support team and provide photos of the installation, as well as screenshots showing the abnormal wind speed data? This information will help our engineers further investigate and follow up on the issue. email: [email protected]

1 Like