SenseCap indicator - Error after flash example. I can't flash initial image anymore

Hi, I got a new SenceCap Indicator and I am trying to flash the Home Assistant example.
I was able to build and flash it with a few hours lost with idf.py commands. The device was not configured as esp32s3. I changed the env variable and built.
But I have this issue at boot - LCD memory allocation errors:

I (638) i2c_bus: i2c0 bus inited
I (642) bsp boards: detecting board SenseCAP_Indicator
I (648) bsp boards: Detected board: [SenseCAP_Indicator]
I (659) gpio: GPIO[38]| InputEn: 1| OutputEn: 0| OpenDrain: 0| Pullup: 1| Pulldown: 0| Intr:0 
E (664) lcd_panel.rgb: lcd_rgb_panel_alloc_frame_buffers(156): no mem for frame buffer
E (672) lcd_panel.rgb: esp_lcd_new_rgb_panel(285): alloc frame buffers failed

I played with the idf.py menuconfig without success.

I tried other examples, with the same issue. It looks like a config issue during build.

I have issues with the Patch as well. With esp-idf release 5.0, I can’t apply the patch

PS> git apply --whitespace=fix D:\Dev\RPI\SenseCap\SenseCAP_Indicator_ESP32\tools\patch\release5.0_psram_octal_120m.patch
D:/Dev/RPI/SenseCap/SenseCAP_Indicator_ESP32/tools/patch/release5.0_psram_octal_120m.patch:461: trailing whitespace.
# Legacy, F8R8, Flash 120M DDR, PSRAM disable
D:/Dev/RPI/SenseCap/SenseCAP_Indicator_ESP32/tools/patch/release5.0_psram_octal_120m.patch:462: trailing whitespace.

D:/Dev/RPI/SenseCap/SenseC

AP_Indicator_ESP32/tools/patch/release5.0_psram_octal_120m.patch:463: trailing whitespace.
CONFIG_SPI_FLASH_USE_LEGACY_IMPL=y
D:/Dev/RPI/SenseCap/SenseCAP_Indicator_ESP32/tools/patch/release5.0_psram_octal_120m.patch:464: trailing whitespace.
CONFIG_ESPTOOLPY_OCT_FLASH=y
D:/Dev/RPI/SenseCap/SenseCAP_Indicator_ESP32/tools/patch/release5.0_psram_octal_120m.patch:465: trailing whitespace.
CONFIG_ESPTOOLPY_FLASH_SAMPLE_MODE_DTR=y
error: patch failed: components/spi_flash/spi_flash_timing_tuning.c:230
error: components/spi_flash/spi_flash_timing_tuning.c: patch does not apply

How can I solve this?
Thanks.

I re-installed the esp-idf 5.0 and patch worked.
I still have the same issue with memory allocation

E (664) lcd_panel.rgb: lcd_rgb_panel_alloc_frame_buffers(156): no mem for frame buffer
E (672) lcd_panel.rgb: esp_lcd_new_rgb_panel(285): alloc frame buffers failed

I played with all configs in idf.py menuconfig and installed esp-idf 5.1.
Now I can compile, flash and it works. BUT I have a very weird display. The image on the device is flickering and is unusable. This might be related to some frequency issues but I can’t find it.
What a pain to just test an example for a brand-new device using vendors repo… I am far from customizing the device for my needs.

This looks like dead community.
I resolved my prob (few hours lost)

Hi, we apologize for not being aware of your information because the technical support engineers have a rest time on weekends. Our working hours are from 9:00 to 18:00 (Beijing time) from Monday to Friday.

Thanks for the information. Still the community is very quiet on Discord and Forum.
Hopefully supporting engineers will be more helpful during the week.

Have a good day.

Hi,
image
Good morning/evening, you can @Meilily, she is in charge of tech support for SenseCap.She may be busy with something else