SenseCAP 4G Sensor Hub Maximum Voltage Input

What is the maximum DC Voltage input for the 4G Sensor Hub? Can I use a solar panel that has an open circuit voltage up to 21V?

Thanks

The Sensor Hub is powered by 12V DC, so if you need solar power, you have to buy a solar system(solar panel + battery) that outputs 12V DC.

hi i need to know how to connect solar panel and with what connector ?

I think you should create a new thread for your question. This thread is 4 years old.

Please use the WM13-6pin Aviation Connector to connect the solar panel. The pin configuration is as follows:

  • Pin 2: Power +

  • Pin 5: Power -

Please make sure the polarity is correct when connecting the solar panel to avoid any potential damage to the device.