Seeeduino Xiao USB port stopped being recognized by windows 10

I just started to use my Xiao SamD (or at least trying to).

  • I plugged in the board as received from Seeeduino.

  • I programmed a demo for an LCD.

  • Immediately after the download succeeded windows popped up with a message something like " the last device connected in not recognized by windows" (Win 11 pro).

  • What’s funny is the popup would occur every 10 seconds or so. I’ve never seen such an action from Windows.

  • I then deleted the grayed out com port, the Xiao board was again recognized, I double shorted the reset and got into the boot (orange) mode.

  • Programmed the board with the “blink without delay” example.

  • Went right back to cannot recognize.

Is there a cure for this or do I just scrap these boards?

Thanks

John