Seeeduino Xiao RP disconnects from the COM port whenever I try to upload a sketch from Arduino IDE

Hi Jostar,

The thing is that I don’t want the Xiao to appear as a disk drive, I want to program in in dev mode and upload a sketch. I’ve done the boot mode and it appears as a disk driver but again, this is not what I want. Maybe I’m supposed to load some kind of firmware on the device in order for it to work as I want? I’m a little lost in that sense, sorry if the question sounds a bit silly.