Seeeduino V4.2, SD Card Shield V4 and Grove Base Shield V2.0

Can I stack on top of Seeeduino V4.2, SD Card Shield V4 and Grove Base Shield V2.0? I wish to save data from sensors.

yes, you can use that, since the Grove Base Shield in default doest requires SPI lines, and the SD card shield uses the SPI lines, so we can use that without any problem.