Help! I bought several seeeduino v4.2 and optical encoders with plans to use them in a class. When I follow instructions here
I do not see an option to add my board as an option, so that I can select it in board manager, even though the description shows that I should be seeing it. I do see options for other seeed boards. I am using an ubuntu computer but have the same problem with windows.