Hi everybody !
How to download firmware on communications ship on Seeeduino V3.0 ?
I have a Atmel AVRISP STK500 USB ISP Programmer (this one : seeedstudio.com/wiki/index.p … Programmer) ?
On arduino board, there is a connector beside USB connector, is it the same than “UART” connector (without pin) beside ICSP connector on Seeeduino V3.0 ?
The UART port beside the ICSP port of Seeeduino is not the same function of the connector beside the USB connector of Arduino.
Jacket
Thanks for your response.
I’d could repair firmware on USB communications ship on “real” Arduino, is it not possible on Seeeduino ?
Maybe you wanna burn the boot loader “UNO” to Seeeduino? Of course, you can.
USB communication firmware is not the same than bootloader.
I’d tried to put Arduino bootloader on Seeeduino, it works, but there is another firmware for chip communication (on Arduino, it can be changed to do a usb HID with arduino board)