Sorry to bother with such a simple question, I just want to make sure I don’t fry my Seeeduino. I have the v1.1 and I want to use external power via de JST connector. The one I have has no +/- marking but looking at newer versions and the board it seems to me that + is towards the edge of the board and GND towards the regulator. Is this true?
I am asking because I was sure this was the case until I saw this cable seeedstudio.com/depot/dc-jac … Path=79_83 which seems to be the other way.
Can you please clarify for me on Seeeduino v1.1 which is the + and which is GND on the white connector? Thanks!