Hello,
I just received my Seeeduino Stalker 2.1 kit, as well as a Circuits@Home USB Host Shield to use with it.
I’m interested in adding a GPS Bee to my project, but based on where the USB connector is on the shield, it looks like the GPS Bee might not fit.
Has anyone tried this? Can you tell if it would fit or not?
Thanks,
Vitorio
deray
March 30, 2012, 10:17am
2
You need XBee® Shield but not USB Host Shield.
seeedstudio.com/depot/xbee%C … th=132_134
Best regards,
Deray
No, I’m attaching a USB device to the Seeeduino Stalker, so I really do need the USB Host Shield. So along with the size of the host shield, there is also the USB device I’m attaching.
Will a GPS Bee also fit in this configuration?
Thanks.
deray
March 31, 2012, 2:22am
4
Yes, the GPS Bee fit in this configuration.Just put it in BEE label position on the board.