Hi,
it would be nice to have jumpers for the MISO, MOSI, SS and SCK. The Atmega 328 (used in 2009 or Uno) has them routed to the pins 10-13. The Atmega 2560 (also the 1280) has it on the pins 50-53. So it would be nice if we could use jumpers for these four pins and can easiely decide if we want to use the pins 10-13 of the Seeeduino board as the regular pins 10-13 or as the MISO, MOSI, SS and SCK.
Regards, Nils.