Hello,
Is it possible to power the Seeeduino Mega v3.0 with an external 5V source? Should I connect this 5V directly to the 5V and GND headers?
When done so, can I then connect the USB or will this break the board or USB port?
Note: A similar question was asked for the 1.23 version but that answer cannot be applied to version 3.0 because the power circuits between these versions are quite different.
thanks in advance,
Hans