I have a new PC and I cannot get the Seeeduino Lotus to work. It worked fine on my last pc.
I installed the drivers, and when I try to upload, I get error:
No device found on cu.SLAB_USBtoUART
An error occurred while uploading the sketch
I have selected Seeeduino Lotus - Cortex - M0+ as the board.
Port is /dev/cu.SLAB_USBtoUART
Programer is AVR ISP.
It does not allow me to select baud rate or other information, I only have Board and Port for this board.
I tried uploading to NodeMCU and that works, so the driver is ok.
Please advise.
Hi there,
Seeeduino Lotus 1.0 works at Windows Operating System ONLY. Seeeduino Lotus 1.1 works with Window and Mac.
which version do you have? thanks
Hi, I have 1.1 version. I can provide photo for proof if needed.