I’m trying to integrate Seeeduino LoRaWAN to TTN through using my own RAK7249 gateway which is registered and active on the TTN network successfully.
The gateway is programmed for AU915 second-band settings. Namely it’s using uplink channels 8-15 and 65 (916.8-918.2 MHz and 917.5 MHz).
I can see that the Join request is sent to the TTN and a response on 923.3 MHz (The downlink frequency) arrives but it is never acknowledged by the Seeeduino. See below:
Seeeduino Log:

Gateway packet logger:

The arduino code:
[code]#include <LoRaWan.h>
unsigned char data[10] = {1, 2, 3, 4, 5, 6, 7, 8, 9, 0xA,};
char buffer[256];
void setup(void)
{
Serial.begin(115200);
delay(5000);
lora.init();
memset(buffer, 0, 256);
lora.getVersion(buffer, 256, 1);
Serial.print(buffer);
memset(buffer, 0, 256);
lora.getId(buffer, 256, 1);
Serial.print(buffer);
// void setId(char *DevAddr, char *DevEUI, char *AppEUI);
lora.setId(NULL, "00D433CC276F57D7", "70B3D57ED0024CCA");
// setKey(char *NwkSKey, char *AppSKey, char *AppKey);
lora.setKey(NULL, NULL, "32B31BDCB5CBFC4B04500D1BEA4F2F3E");
lora.setDeciveMode(LWOTAA);
lora.setDataRate(DR2, AU915);
lora.setChannel(8, 916.8, DR0, DR5);
lora.setChannel(9, 917.0, DR0, DR5);
lora.setChannel(10, 917.2, DR0, DR5);
lora.setChannel(11, 917.4, DR0, DR5);
lora.setChannel(12, 917.6, DR0, DR5);
lora.setChannel(13, 917.8, DR0, DR5);
lora.setChannel(14, 918.0, DR0, DR5);
lora.setChannel(15, 918.2, DR0, DR5);
lora.setReceiceWindowFirst(0, 923.3);
lora.setReceiceWindowFirst(1, 923.9);
lora.setReceiceWindowFirst(2, 924.5);
lora.setReceiceWindowFirst(3, 925.1);
lora.setReceiceWindowFirst(4, 925.7);
lora.setReceiceWindowFirst(5, 926.3);
lora.setReceiceWindowFirst(6, 926.9);
lora.setReceiceWindowFirst(7, 927.5);
lora.setReceiceWindowSecond(923.3, DR8);
lora.setDutyCycle(false);
lora.setJoinDutyCycle(false);
lora.setPower(14);
while (!lora.setOTAAJoin(JOIN));
}
void loop(void)
{
bool result = false;
result = lora.transferPacket("{test: '1234', test2: '234'}", 10);
//result = lora.transferPacket(data, 10, 10);
if (result)
{
short length;
short rssi;
memset(buffer, 0, 256);
length = lora.receivePacket(buffer, 256, &rssi);
if (length)
{
Serial.print("Length is: ");
Serial.println(length);
Serial.print("RSSI is: ");
Serial.println(rssi);
Serial.print("Data is: ");
for (unsigned char i = 0; i < length; i ++)
{
Serial.print("0x");
Serial.print(buffer[i], HEX);
Serial.print(" ");
}
Serial.println();
}
}
}<e>[/code]</e></CODE>
Any help in this matter will be very much appreciated. Thank you!