Hello,
I find that the default opkg repository of Seeeduino Cloud (Linino Dogstick) appears to miss several packages that I wish to use. That is, I cannot do opkg update and opkg install those packages.
I have two questions:
-
Is it possible to replace Seeeduino Cloud’s openwrt image (now it’s seeed-build–v1.3.4) entirely by Arduino Yun’s image (e.g. from http: //arduino.cc/en/pmwiki.php?n=main/software)? That is would the two boards be 100% image compatible ?
-
If 1) is not possible, I wish to build all the missing packages from sources. Are there any instructions that are similar to http: //fibasile.github.io/arduino-yun-custom-buildroot.html but specifically aim for the Seeeduino Cloud ?
(remove the extra space in the URL before you browse them).
Thanks very much in advance,
Regards,
Apinun