Seeediuno 4.3 and DTH22

I used the default code, which showed up after I added the library.
// Example testing sketch for various DHT humidity/temperature sensors

// Written by ladyada, public domain

#include “Grove_Temperature_And_Humidity_Sensor.h”

// Uncomment whatever type you’re using!

//#define DHTTYPE DHT11 // DHT 11

#define DHTTYPE DHT22 // DHT 22 (AM2302)

//#define DHTTYPE DHT21 // DHT 21 (AM2301)

//#define DHTTYPE DHT10 // DHT 10

//#define DHTTYPE DHT20 // DHT 20

/Notice: The DHT10 and DHT20 is different from other DHT sensor ,it uses i2c interface rather than one wire*/

/So it doesn’t require a pin./

#define DHTPIN 2 // what pin we’re connected to(DHT10 and DHT20 don’t need define it)

DHT dht(DHTPIN, DHTTYPE); // DHT11 DHT21 DHT22

//DHT dht(DHTTYPE); // DHT10 DHT20 don’t need to define Pin

// Connect pin 1 (on the left) of the sensor to +5V

// Connect pin 2 of the sensor to whatever your DHTPIN is

// Connect pin 4 (on the right) of the sensor to GROUND

// Connect a 10K resistor from pin 2 (data) to pin 1 (power) of the sensor

#if defined(ARDUINO_ARCH_AVR)

#define debug  Serial

#elif defined(ARDUINO_ARCH_SAMD) || defined(ARDUINO_ARCH_SAM)

#define debug  SerialUSB

#else

#define debug  Serial

#endif

void setup() {

debug.begin(115200);

debug.println("DHTxx test!");

Wire.begin();

/*if using WIO link,must pull up the power pin.*/

// pinMode(PIN_GROVE_POWER, OUTPUT);

// digitalWrite(PIN_GROVE_POWER, 1);

dht.begin();

}

void loop() {

float temp_hum_val[2] = {0};

// Reading temperature or humidity takes about 250 milliseconds!

// Sensor readings may also be up to 2 seconds 'old' (its a very slow sensor)

if (!dht.readTempAndHumidity(temp_hum_val)) {

    debug.print("Humidity: ");

    debug.print(temp_hum_val[0]);

    debug.print(" %\t");

    debug.print("Temperature: ");

    debug.print(temp_hum_val[1]);

    debug.println(" *C");

} else {

    debug.println("Failed to get temprature and humidity value.");

}

delay(1500);

}
Sean