@Citric Below are the errors I am getting. Library’s git page mentions that it is only compatible with ATmega microcontrollers. I am new to Arduino development and it would be awesome if someone can navigate me.
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp: In function 'void toneAC(long unsigned int, uint8_t, long unsigned int, uint8_t)':
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:23:5: error: 'TIMSK1' was not declared in this scope
23 | TIMSK1 |= _BV(OCIE1A); // Activate the timer interrupt.
| ^~~~~~
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:23:19: error: 'OCIE1A' was not declared in this scope
23 | TIMSK1 |= _BV(OCIE1A); // Activate the timer interrupt.
| ^~~~~~
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:23:15: error: '_BV' was not declared in this scope
23 | TIMSK1 |= _BV(OCIE1A); // Activate the timer interrupt.
| ^~~
In file included from XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:8:
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp: In function 'void toneAC_playNote(long unsigned int, uint8_t)':
XXXXX/xiao/libraries/toneAC/src/toneAC.h:106:23: error: 'DDRB' was not declared in this scope
106 | #define PWMT1DREG DDRB
| ^~~~
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:31:3: note: in expansion of macro 'PWMT1DREG'
31 | PWMT1DREG |= _BV(PWMT1AMASK) | _BV(PWMT1BMASK); // Set timer 1 PWM pins to OUTPUT (because analogWrite does it too).
| ^~~~~~~~~
XXXXX/xiao/libraries/toneAC/src/toneAC.h:104:24: error: 'DDB1' was not declared in this scope; did you mean 'B1'?
104 | #define PWMT1AMASK DDB1
| ^~~~
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:31:20: note: in expansion of macro 'PWMT1AMASK'
31 | PWMT1DREG |= _BV(PWMT1AMASK) | _BV(PWMT1BMASK); // Set timer 1 PWM pins to OUTPUT (because analogWrite does it too).
| ^~~~~~~~~~
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:31:16: error: '_BV' was not declared in this scope
31 | PWMT1DREG |= _BV(PWMT1AMASK) | _BV(PWMT1BMASK); // Set timer 1 PWM pins to OUTPUT (because analogWrite does it too).
| ^~~
In file included from XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:8:
XXXXX/xiao/libraries/toneAC/src/toneAC.h:105:24: error: 'DDB2' was not declared in this scope; did you mean 'D2'?
105 | #define PWMT1BMASK DDB2
| ^~~~
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:31:38: note: in expansion of macro 'PWMT1BMASK'
31 | PWMT1DREG |= _BV(PWMT1AMASK) | _BV(PWMT1BMASK); // Set timer 1 PWM pins to OUTPUT (because analogWrite does it too).
| ^~~~~~~~~~
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:33:27: error: 'CS10' was not declared in this scope
33 | uint8_t prescaler = _BV(CS10); // Try using prescaler 1 first.
| ^~~~
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:36:21: error: 'CS12' was not declared in this scope
36 | prescaler = _BV(CS12); // Set the 256 prescaler bit.
| ^~~~
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:40:3: error: 'ICR1' was not declared in this scope; did you mean 'IR1'?
40 | ICR1 = top; // Set the top.
| ^~~~
| IR1
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:41:7: error: 'TCNT1' was not declared in this scope
41 | if (TCNT1 > top) TCNT1 = top; // Counter over the top, put within range.
| ^~~~~
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:42:3: error: 'TCCR1B' was not declared in this scope
42 | TCCR1B = _BV(WGM13) | prescaler; // Set PWM, phase and frequency corrected (top=ICR1) and prescaler.
| ^~~~~~
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:42:16: error: 'WGM13' was not declared in this scope
42 | TCCR1B = _BV(WGM13) | prescaler; // Set PWM, phase and frequency corrected (top=ICR1) and prescaler.
| ^~~~~
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:43:3: error: 'OCR1A' was not declared in this scope
43 | OCR1A = OCR1B = top / _tAC_volume[volume - 1]; // Calculate & set the duty cycle (volume).
| ^~~~~
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:43:12: error: 'OCR1B' was not declared in this scope
43 | OCR1A = OCR1B = top / _tAC_volume[volume - 1]; // Calculate & set the duty cycle (volume).
| ^~~~~
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:44:3: error: 'TCCR1A' was not declared in this scope
44 | TCCR1A = _BV(COM1A1) | _BV(COM1B1) | _BV(COM1B0); // Inverted/non-inverted mode (AC).
| ^~~~~~
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:44:16: error: 'COM1A1' was not declared in this scope
44 | TCCR1A = _BV(COM1A1) | _BV(COM1B1) | _BV(COM1B0); // Inverted/non-inverted mode (AC).
| ^~~~~~
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:44:30: error: 'COM1B1' was not declared in this scope
44 | TCCR1A = _BV(COM1A1) | _BV(COM1B1) | _BV(COM1B0); // Inverted/non-inverted mode (AC).
| ^~~~~~
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:44:44: error: 'COM1B0' was not declared in this scope
44 | TCCR1A = _BV(COM1A1) | _BV(COM1B1) | _BV(COM1B0); // Inverted/non-inverted mode (AC).
| ^~~~~~
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp: In function 'void noToneAC()':
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:48:3: error: 'TIMSK1' was not declared in this scope
48 | TIMSK1 &= ~_BV(OCIE1A); // Remove the timer interrupt.
| ^~~~~~
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:48:18: error: 'OCIE1A' was not declared in this scope
48 | TIMSK1 &= ~_BV(OCIE1A); // Remove the timer interrupt.
| ^~~~~~
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:48:14: error: '_BV' was not declared in this scope
48 | TIMSK1 &= ~_BV(OCIE1A); // Remove the timer interrupt.
| ^~~
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:49:3: error: 'TCCR1B' was not declared in this scope
49 | TCCR1B = _BV(CS11); // Default clock prescaler of 8.
| ^~~~~~
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:49:17: error: 'CS11' was not declared in this scope
49 | TCCR1B = _BV(CS11); // Default clock prescaler of 8.
| ^~~~
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:50:3: error: 'TCCR1A' was not declared in this scope
50 | TCCR1A = _BV(WGM10); // Set to defaults so PWM can work like normal (PWM, phase corrected, 8bit).
| ^~~~~~
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:50:17: error: 'WGM10' was not declared in this scope
50 | TCCR1A = _BV(WGM10); // Set to defaults so PWM can work like normal (PWM, phase corrected, 8bit).
| ^~~~~
In file included from XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:8:
XXXXX/xiao/libraries/toneAC/src/toneAC.h:107:23: error: 'PORTB' was not declared in this scope
107 | #define PWMT1PORT PORTB
| ^~~~~
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:51:3: note: in expansion of macro 'PWMT1PORT'
51 | PWMT1PORT &= ~_BV(PWMT1AMASK); // Set timer 1 PWM pins to LOW.
| ^~~~~~~~~
XXXXX/xiao/libraries/toneAC/src/toneAC.h:104:24: error: 'DDB1' was not declared in this scope; did you mean 'B1'?
104 | #define PWMT1AMASK DDB1
| ^~~~
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:51:21: note: in expansion of macro 'PWMT1AMASK'
51 | PWMT1PORT &= ~_BV(PWMT1AMASK); // Set timer 1 PWM pins to LOW.
| ^~~~~~~~~~
XXXXX/xiao/libraries/toneAC/src/toneAC.h:105:24: error: 'DDB2' was not declared in this scope; did you mean 'D2'?
105 | #define PWMT1BMASK DDB2
| ^~~~
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:52:21: note: in expansion of macro 'PWMT1BMASK'
52 | PWMT1PORT &= ~_BV(PWMT1BMASK); // Other timer 1 PWM pin also to LOW.
| ^~~~~~~~~~
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp: At global scope:
XXXXX/xiao/libraries/toneAC/src/toneAC.cpp:55:4: error: expected constructor, destructor, or type conversion before '(' token
55 | ISR(TIMER1_COMPA_vect) { // Timer interrupt vector.
| ^
Compilation error: exit status 1