Seeed XIAO BLE nRF52840 Sense giving bad gyroscope data

Notes from the Data Sheet… FYI 1LSb = 70 mdps at ±2000 dps full scale.

  1. Typical specifications are not guaranteed.
  2. Measurements are performed in a uniform temperature setup.
  3. Values after soldering.
  4. RND (rate noise density) mode is independent of the ODR and FS setting.
  5. Gyro noise RMS is independent of the ODR and FS setting.
  6. Noise density in HP mode is the same for all ODRs

Good Stuff,
HTH
GL :slight_smile: PJ
try this also. Does it give the proper orientation output?