Cleaning build area…
make -j4 KERNELRELEASE=6.6.47+rpt-rpi-v8 -C /lib/modules/6.6.47+rpt-rpi-v8/build M=/var/lib/dkms/seeed-voicecard/0.3/build…
Eventually hangs the pizero w2, off/on, uninstall, install same results.
Cleaning build area…
make -j4 KERNELRELEASE=6.6.47+rpt-rpi-v8 -C /lib/modules/6.6.47+rpt-rpi-v8/build M=/var/lib/dkms/seeed-voicecard/0.3/build…
Eventually hangs the pizero w2, off/on, uninstall, install same results.
Hi,
It looks like you are installing this library:
May I know which Raspberry Pi hardware and which version of Raspberry Pi OS you are using?
By “pizero w2”, do you mean Raspberry Pi Zero 2 W?
Linux pizero4 6.6.47+rpt-rpi-v8 #1 SMP PREEMPT Debian 1:6.6.47-1+rpt1 (2024-09-02) aarch64 GNU/Linux
Raspberry Pi Zero 2W fresh from Adafruit. I have two o the respeaker/seeed-voicecards on two identical PI Zero 2W. It took many reinstalls on the first one and Finally got it to work. Second one never finishes the build script. What can I copy from one system to the other to just make make it work?
Trying this on the next install.sh
sudo loginctl enable-linger
Any detail logs or screenshots after executing the ./install.sh?