"Seeed nRF52 Boards" update to 1.1.3 causes compile error

After upgrade of “Adafruit nRF52” boards to 1.5.0, seeed entries in the Adafruit nRF52 boards, as obtained with the earlier trick, were gone. So, I used again the official way to install it but stand with 1.1.1 version, as done by @parasquid . It is more or less OK. I’m still loosing the board quite often and have to double-click the reset button to find it back.

1 Like