My Seeduino Cloud board has been working fine for the past few weeks, but suddenly today I was unable to find it in my Serial Ports menu in the Arduino IDE. I tried holding the reset button on the board to reset it, but this did not seem to fix the problem. I can see the LEDs on the board lighting up when I connect the board to my MacBook, meaning that the board is receiving power, and I can SSH (Using the IP address from the Network Port) into the board. How can I fix this problem? Thanks in advance!
Is it because you upgraded your MacBook to MacOS 15? If so, you’ll have to wait for Appla to update. @jksram